Get Support Now

  

Firmware Upgrade Wizard (FUW)

Directions

  1. Download the upgrade file(.exe) to a temporary folder on the same drive as FactoryTalk View ME.
  2. Run the upgrade file(.exe) installation procedure. The new FUW will be installed in the FactoryTalk View ME directory.
    The Firmware Upgrade Package (.FUP) files will be installed into the directory specified during the installation procedure.
  3. Launch the FUW and follow-up the wizard directions. For additional help, download the FUW video

  4. FUW Tutorial Video

For PanelView Plus & PanelView Plus CE 700-1500 upgrades from ME3.0 to ME3.1, contact your local AB distributor.

Upgrade Media catalog numbers:

  • PanelView Plus (700-1500) 2711P - RU310
  • PanelView Plus CE (700-1500) 2711P - RU310

A "System Check" will automatically launch during bootup on the PanelView Plus and PanelView Plus CE 700-1500 terminals (firmware 3.20.05 or later) and PanelView Plus Compact 1000 to help ensure the integrity of your data.Consult the release notes on this web page, or once the FUP has been installed, the releasenote named "Release Note XX.XX.XX.rtf" The release note may also be in a PDF format, and reside in the "RSView Enterprise" directory (..\Rockwell Software\RSView Enterprise) of the RSView install.

For Panelview Plus 6 and Panelview Plus 6 with Extended Feature Click here -> FactoryTalk View ME 6.0

Note: The 4.00.00 Release is only compatible with FactoryTalk View Studio 4.0
         PanelView Plus CE (PVP CE) and VersaView CE (VV CE) firmware is compatible.

For firmware releases not listed on this page, please contact technical support.

A FactoryTalk ViewPoint ME Add-In for FactoryTalk View Studio is required to create web applications for PanelView Plus. For more information and installation instructions click here. For download location click here.

FactoryTalk View ME Platforms Communication Card Firmware
  ME 5.1 Releases ME 5.0 Releases ME 4.0 Releases ME 3.2 Releases DevicelNet Upgrades ControlNet Upgrades
AFS Date and Info 03/23/2012 08/13/2010 05/13/2009 05/13/2009 02/07/2007 02/07/2007
FactoryTalk View ME 5.10.08 5.00.09 4.00.15 3.20.11 3.016 3.10, 4.10
ENGLISH
Release Notes Release Note Release Note Release Note Release Note    
PVPLUS 700-1500 Download RSView Utility Download RSView Utility Download RSView Utility Download RSView Utility Download RSView Utility Download RSView Utility
PVPCE 700-1500 Download RSView Utility Download RSView Utility Download RSView Utility Download RSView Utility Download RSView Utility Download RSView Utility
PVPlus 400/600 Download RSView Utility Download RSView Utility Download RSView Utility Download RSView Utility Download RSView Utility Download RSView Utility
PVPlus Compact 400/600 Download RSView Utility          
PVPlus Compact 1000 Download RSView Utility          
PSA Attention: Important product information. Please click and take the appropriate action as identified in this communication.